Part Number: TPS7A4001
Other Parts Discussed in Thread: TL783, TPS7A43
Hi
By looking at the spec. of TPS7A4001, this LDO can only support up to 50mA output current. However, the application will need 15V/60mA output.
Not sure if TPS7A4001 can meet the spec. If not, may I have your support to provide the suggestion?
Here is the spec.
- Vin Max: 80V
- Vout: 15V
- Iout Max: 60mA~100mA
- Thermal shutdown
- Current shutdown
Thanks.