Other Parts Discussed in Thread: TPS63802
Hi ,
We are using BQ25616 for charging the single Li-ion battery. Along with BQ25616, we are using the TPS63802 Converter for generation of 3.3V.
TPS get input from the Sys node of charger IC. Please see the schematic below,
We are using the BB converter in PFM mode.
When the device is connected to power source, during the charging of the battery we see variation (instead of DC current, a saw tooth waveform) in the charging current. Please see below waveform
Variation of charging current at termination current range:
Termination current with BB in PFM mode:
Termination Current with BB in PWM mode:
Our Understanding:
In PFM mode, BB converter switches on/off the converter based on the load. This causes a change in the voltage at the input of BB, which is Vsys. Vsys voltage is used to charge the battery and hence the variation in the charging current.
Is our understanding correct ?
Questions:
1. Since the Battery current is regulated, why charger IC is not able to maintain constant current ?
2. How does the charger IC detects the termination / pre-charge current ? current might be toggling above and below the threshold?
3. Is this kind of charging current acceptable for Li-ion batteries ?
4. How can we improve the charging current or make sure the PFM mode does not affect the charging current ?