Hi,
I am using the bq20z80 and bq29312 for an project.
By reading documentations I did not found this information:
Is the Dicharge FET is turned off when the circuit going in sleep with NR=1 ?
Thanks,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Yes, DSG FET is off in sleep mode with NR=1 or NR =0.
My customer would like a battery with low power consumption and dicharge feature still active.
Is there any solution to get a low power consumption (with the BQ29312 & BQ20z80) less than 60µA (Averaged) and voltage on the output ?
The aim will to allow a dicharge, and so a wake up, without using /PRES SLEEP pins.
Discharge is active at normal mode only. You can enable sleep, the gauge will wake up when current > wake current.
The current consumption is then switch between normal and sleep mode. The actual average current consumption will depend on the application.