Dear Sir,
I have designed the footprint of TPSM82822 as follows, please help me to check whether it is OK, thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Sir,
I have designed the footprint of TPSM82822 as follows, please help me to check whether it is OK, thanks!
Hi Hung-liang,
You can already download the correct footprint here https://vendor.ultralibrarian.com/TI/embedded/?gpn=TPSM82822&package=SIL&pin=10&sid=0180b6ac05b300ac2bd5b5bc06a805073012806b00bd0&c=1
You can choose the format based on your CAD software.
Best regards,
Varun
Hi Varun,
Thanks, the pad dimession in the file is 0.25mm*0.65mm.
But I saw the pad dimession in the datasheet is (0.2~0.3)mm * (0.6~0.7)mm
Could I have the pad dimession as 0.35mm*0.75mm to cover whole pad?
Hi Hung-liang,
The typical device pad size should be 0.25mm*0.65mm, and that's why the land pattern also has the same dimensions. It is recommended to stick to this as only this has been tested and qualified.
Best regards,
Varun