Hi support team,
Can the PGOOD pin of LMR16030PDDAR be floating?
Can the SS pin of LMR16030SDDAR be a floating?
If both of the above are possible, is it possible to replace LMR16030PDDAR and LMR16030SDDAR?
Even if the SS of LMR16030SDDAR can be floated, LMR16030PDDAR has an internal soft start, so there will be a difference in soft start time, which will be a problem.
Is it possible to connect a SS capacitor to the PGOOD pin of LMR16030PDDAR?
Set the CSS of LMR16030SDDAR to 16nF, set the soft-start time to 4ms, and set it to the internal soft-start time of LMR16030PDDAR.
Regards,
Dice-K