Other Parts Discussed in Thread: TPS61041
TPS61041-Q1 has load current rating of 250mA, I need to design a circuit with load current 120mA, but with the calculation which was mentioned in
Datasheet, I'm not able to meet 120mA, seems like Inductor is not playing much role in load current.
with higher inductance maximum switching frequency is getting reduced thus the load current,
Vin(min) = 3.3 V
Vin(typ)= 3.3V
Vout= 9V
Will you please provide the calculation for 120mA Load current ?
- Thankyou