Other Parts Discussed in Thread: TPS61094
Please help my customer's jumper setting as see Page#7 setting.
JP1: Short 1-2
JP2: Short 1-2
JP3: 1.7V
JP4: 0mA Disable charge
JP5: 3.0V
J11,J12: Set both high.
input Battery : CR2025R This is not re-chargeable battery.
VIN-J1 === J5 Battery VINmin 2.5V VIN MAX 3.6V
VOUT setting = 3V
OUTPut current 10mA max/ 20uA at sleep mode (10ma at 2sec during 5min idling time. then sleep time 20uA)