Other Parts Discussed in Thread: UC2901, UC2706,
Hi team,
I am designing a DC DC Push-Pull converter with 22V to 34V input range, 280V output with 0.7A Load current. I have selected UC2842 as a PWM controller, UC2706 to convert single drive signal to two drive signal, and UC2901 as a isolation feedback controller. My transformer turns ratio is 1:18.
- I am able to achieve fixed 280V output with the input voltage variation from 22V to 34V but only under no load condition.
- My output voltage is not fixed it will vary +/- 15V to 20V under load condition, meaning my feedback compensation to UC2842 is not working properly.
- I am facing an issue in feedback compensation at UC2842. How to tune feedback compensation values for UC2842 with respect to boost application?
- Is there any calculation sheet available for compensation tuning for UC2842 ?
- Is UC2842 will works for such a high transformer ratio application?
Thanks & regards,
Karthik Venkateshaiah.