Dear,
I met a problem in the simulation by LTspice.
Short description of the circuit:
There's a current limitation (10mA) after the Voltage Source, the input side of TPS7A24 has 470uF capacitor, the output side has 20uF capacitor.
Problem in the simulation result:
The input voltage was stuck at ~2.1V and cannot rise, so there's no voltage output, it seems there's some kind of current limitation (ilim) in the LDO model, but how can I do with Cout=20uF?
Thanks.
Pls see the screen shot of the simulation below (the blue line is the current through Cout) and the .lib file and the source file which I used.