Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54232: Searching TI solution

Part Number: TPS54232
Other Parts Discussed in Thread: TPS629210-Q1, TPS562202

Hi Team

There is good new that we could DIN our device!
Because customers have price considerations, whether there are lower-priced products that can be recommended to customers ?THX

Spec as following :
Vin=5V
Vo=3.3V
Io=1A
Automotive

  • Hi Kygo

    Does customer want to use an automotive device? TPS54232 is not the automotive solution. If customer prefer an automotive solution, I would recommend TPS629210-Q1. Otherwise, I would recommend TPS562202/7.

    Is there any special concern here? Like solution size, efficiency, load transient, output ripple, EMI, etc..?

    BR

    Ruby