Other Parts Discussed in Thread: UCC24612, UCC24650, UCC2897A
Hi team,
My customer has following questions on this chip:
1.Is UC28780 suitable to control the active dual-position flyback chip to be used in a 70W 24/24V isolated dcdc circuit (the upper and the lower switch are MOS tubes with Vgs(th)=4V) 2.In the case of inputting 24V±20%, can the auxiliary winding on the VDD input side be canceled and directly connected to the input terminal? Will it have an impact on the sampling of the VS terminal and thus have a great impact on the output overvoltage feedback loop?
3.In addition to the UCC24612 synchronous rectification chip, are there other synchronous rectification chips for the UCC28780 control chip? (such as UCC24650)
4.Are there any selection requirements for the switch tube in the active filter circuit at the HVG end of the control chip UCC28780?
Thanks for the support!