Other Parts Discussed in Thread: UC28025,
Hi
We use UC28025 today and are looking at the UC28023 and have two questions. One about pin 11 on the UC28023 and one about setting max duty cycle for the UC28023.
- Is pin 11 on UC28023 optional to use? If not used will the ILIM be the same for UC28023 and UC28025? Can it be left unconnected? Looking at "8.2 Functional block diagram" in the datasheet the UC28025 has a 1 volt reference and the UC28023 seems to not have this (if not connected externally). So one could think that a 1 volt external reference is needed when using the UC28023 instead of the UC28025.
- Is it possible to limit the duty cycle as low as 50% on the UC28023?
Best regards
Jonas