Other Parts Discussed in Thread: BQSTUDIO, EV2400, GPCCHEM
Hi,
I'm writing again for a pending problem: RSOC unreliability.
We selected the correct CHEMID, we successfully completed the learning cycle, we correctly configured the parameters, and we followed all the instructions that you proposed also in the previous threads on this forum.
Unfortunately, we are always experiencing the same problem on the RSOC that is drifting after some cycles.
As you can see from the graphs the RSOC (violet line) is diverging respect to the ASOC (green one). A part that reliability of the measure is not good, in addition the BMS stops the charging of the battery with a voltage lower respect to the nominal (8.4). The last cycle of charge is stopped around 7.8V for RSOC 100%.