Hello,
My customer is planning on using the BQ27742-G1 and had a few questions.
- Will the gauge lose accuracy over time?
- As the battery degrades will the gauge be less accurate?
- Does the device need to update and relearn every so often or is the algorithm constantly updating?
- Are there any commands that need to be sent to relearn/update?
- Do the learning cycles need 100% discharge to complete?
- What is the min amount of discharge to ensure highest accuracy?
- If we want to limit users to 80% battery life, then will our fuel gauge be less accurate?
- Ideally, we will want to use 80% of battery life at the beginning then allow the users to use 100% of the battery life after years of use.
Thanks!