This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34110EVM-796: For Lead Acid Battery.

Part Number: BQ34110EVM-796
Other Parts Discussed in Thread: EV2400, BQSTUDIO

Hi Ti 

> I am Using BQ34110EVM-796 attached to ev2400 and connected with BQ studio.

> My battery is LEAD Acid Battery 12V/12 AH.

> Using GPC i had received the   ZIP File as attached ,as per SLUUB45B 

Now How can i generate the GG file for this attached Zip file,  so that i can directly update the data to data memory of BQ studio ?

8877.GPC_report.zip

  • Hello Ravi,

    The report shows CEDV parameters resulting from the fit.

    Use bqStudio data memory tab to set the parameter values in "CEDV Profile" under "Gas Gauging". Then export a GG file.

    You can also edit the GG file in a text editor to use the values from the report.

  • Hi Shirish

    I had tried to enter the values in the data memory. but after entering the values i had clicked read all. then i am getting some error.

    could you  share me any reference  .gg file of lead acid battery.

      

  • Hello Ravi,

    The error is shown at the bottom. Manufacture date is incorrectly set. You can fix this manually by writing that parameter in bqStudio.

    The other red highlight items are an indicator that the values changed from the previous read. Since you imported the GG files, these values are expected to be different. Another "Read All" opertion will remove the red highlight.

  • Hi Shirish 

    Thanks for reply, my issue is resolved

     Problem: Using BQ studio i am Unable to flash the gas gauge parameters to the data memory of IC 

    Solution: By Pressing the commands UNSEALED and UNSEAL FULL ACCESS i am able to flash to data memory of IC.

  • Hi Shirish 

    Thanks for reply, my issue is resolved

     Problem: Using BQ studio i am Unable to flash the gas gauge parameters to the data memory of IC 

    Solution: By Pressing the commands UNSEALED and UNSEAL FULL ACCESS i am able to flash to data memory of IC.

  • Hello Ravi,

    Good to know that your issue is resolved. Thanks for letting us know.