Hi team,
Our customer used LM5069 to design a charge protection circuit consisting of two parts shown below. In their design, the circuit shown in the first picture was used to detected the batteries which they used Vcc_12V to simplify the circuit. If the batteries were detected, the VCC_charger line would connect to 58V voltage source not shown in the picture. And in the second picture there was typical protection circuit based on lm5069,which connected VCC_Charger to the charger circuit.
There was a connecter to connect VCC_Charger shown in the first picture to the VCC_Charger shown in the second picture. According to the resistors shown in the picture, the voltage of VCC_charge was 7.9V((12V-0.7)÷((R53+R57)//(R52+R56+R60)+R46)*(R53+R57)//(R52+R56+R60)=7.9V) without connector. When VCC_Charger in both diagrams was connected ,we can calculate that the voltage of VCC_Charger is 4.9V.
But actually, when VCC_Charger connected in both diagrams ,the voltage of VCC_Charger only maintained at 5V for almost 140ms and then dropped to 3.5V . The wave of entire connection process was shown in the third picture. In addition, when they removed LM5069 and connected VCC_Charger line, the voltage was stable at 5V.
According to the threshold of UVLO and OVLO, LM5069 would not work.
So I want invite you to help to look for the reason why there is s a drop when VCC_Charger is connected with LM5069 on.
Thanks and looking forward to your kind response!
Best Regards,
Nan