Other Parts Discussed in Thread: LM5158-Q1, LM5156-Q1, LM5157, LM5158, LM5156, LM5156EVM-BST, LM5158EVM-BST
Hi Team,
Our customer is considering using LM5157-Q1 in his project and would like to use an EVM to evaluate the device. However, the 3 available EVM only allows Vout up to 12V~20V.
The customer has a solar cell having 42V input with 0.4A current output. and would like to know if the evaluation board for this particular IC can take this input and produce more than 40V.
Is there a workaround to do this? or can you give any alternate IC with available EVM that can accommodate?
Thanks in advance.
Regards,
Marvin