Part Number: TPS54394
Hi,
Pleaes advise if we can connect the VO1 and VO2 and the output current are 6A max,? Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS54394
Hi,
Pleaes advise if we can connect the VO1 and VO2 and the output current are 6A max,? Thanks.
Hi
Amod will reply you tomorrow.
Shuai
Hi Zhang,
No we do not recommend this parallel operation with this control architecture as you have issues with current sharing. You may need to consider a peak current mode device for this type of operation or find another device that works for the conditions. If you want to let us know the Vin, Vout, Iout, etc. and other features that you are looking for, we can recommend alternate devices.
Thanks,
Amod
Hi Amod,
Notes and thanks, we maybe choose other peak current mode device fot this project, thanks.