Other Parts Discussed in Thread: TPSM831D31
Hello Everyone,
I am working on schematic design of TPSM8D6C24 buck- regulator with the below requirement.
The o/p voltage is 0.82V.
1. 0.8159V/0.82V/0.8241V@63A (Want to control through PMBus (I2C) and Hardware (VSEL pin) )
2. The o/p voltage tolerance is 0.5%.
3. Vout Ripple: 30mV
is this regulator supports the tolerance of 0.5%?
Can someone suggest and clarify it? Do you have any other regulator which can support the above requirement?
Your quick response in this regard will be highly appreciable.
Regards
Kapil