Hi expert,
Do you have any data for IDSS max at Ta=85C
Thanks
Muk
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Muk-san,
Thanks for the inquiry. I pulled up the characterization data collected during product development at -55, -25, +25, +75, +125 and +150°C. When I plot this data, I estimate typical IDSS at 85°C is ~225nA and max IDSS is <500nA. These are for guidance and TI only guarantees and tests what is specified in the datasheet. I'm including a link below to a technical article on temperature variation of FET parameters which you may find useful.
Best Regards,
John Wallace
TI FET Applications