Other Parts Discussed in Thread: TLC59116
How to select the value of IREF resistor for the IC for driving 15 LED's.
Forward voltage of led- 3V
forward current- 300 mA
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Hardy,
The led glow will be driven through PWM. Each led has forward current of 300 mA. So as per my understanding, the resistor is not required as maximum current will not cause led damage? i just wanted to understand the equation given in the datasheet. Will the resistor limit the maximum current across all the leds or limit each individual current of led?
Hi Sampan,
For each channel of LP5018, the maximum current capability is 35mA. Here is protection circuit inside each output channel, which limits the current below around 80mA. But setting resistor above 35mA , it is out of datasheet recommendation and will have potential risk.
For such high current application, we do not have a single IC can achieve it. You could take a look of TLC59116, which is a 16- channel device and each channel have 120mA capability. Parallel 3 channels together can support up to 360mA. So that 2 pcs of TLC59116 can support your application.