Hello Everyone,
I am looking for a buck regulator/ Module with below requirement.
The o/p voltage is 0.82V.
1. 0.8159V/0.82V/0.8241V@63A (Want to control through PMBus (I2C) and Hardware (FB/VSEL pin) )
2. The o/p voltage tolerance is 0.5%.
3. Vout Ripple: 30mV
4. Transient Current Load- 30- 50%
Can someone suggest and clarify it? Your quick response in this regard will be highly appreciable.
Regards
Kapil