Other Parts Discussed in Thread: ISO1042,
Lacking a cheap, fast boost controller I am considering a trick to use this device as a simple boost converter from ca. 4V to 5V.
The design is as follows:
Can this work?
My main concern is the start-up or a temporary output short-circuit where the device might go into 100%-PWM and not recover. I try to prevent that with the resistor from the input to the voltage divider, but the behavior for the LDO-function isn't well specified.
Any other suggestions?