Hi Team,
Do we have a single phase inverter with PWM signals controllable by the user using TI microcontrollers?
Parameters : 180-230 v AC to bellow 100 V DC, above 2kW
Thanks.
Regards,
May
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
Do we have a single phase inverter with PWM signals controllable by the user using TI microcontrollers?
Parameters : 180-230 v AC to bellow 100 V DC, above 2kW
Thanks.
Regards,
May
Hi Ryan,
The customer would like to apply different spread spectrum modulation to see the conducted emission reduction of the inverter.
Theywould prefer to vary the switching frequency (for example from 10 kHz to 100 kHz). Also the PWM signals should be controlled externally using TI dsp boards.
The power rating can be as low as 1 kW and the topology can be single phase.
Regards,
May