Hi,
I am designing a 3.6V converter with VIN= 5.5V based on the TPS62160. After producing the board and measure on it, I get a lower voltage than excpected. There is a 600mV difference and this difference gets higher with every batch produced. The FB resistors have 1% tolerances with values not so big to impact the FB accuracy: on the range of 15k as max values.
Do you have any ideas on what might cause this problem?
Thanks in advance for the help?
/Zakaria.