Other Parts Discussed in Thread: TPS65133, TPS65132
Hi Team,
I am using LT1054IP to generate -5V from 5V for op-amp power supply.
The circuit I built is same as datasheet typical aplicaiton, R2 is 102.6k ohm.
The problem is output always lower than input around 0.2V.
when input +5V, out put is around- 4.8V,
input = 5.5V, output =- 5.3V
input =4.7V, output=-4.5V
(Havn't connected load, just placed a LED and 5kohm resister in serial on output)
Could you help advice is this normal? how to get a stable -5V output, thanks in advance!
I