Other Parts Discussed in Thread: TPS63001, , TPS63000
Hi Expert,
May I know what's the difference between TPS6300x family, besides below V/I curve?
Especially, could customer use TPS63002 to replace TPS63001? Thanks.
Regards,
Jared
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jared,
The output voltage of TPS63000/001/002 are different. TPS63000 output voltage is adjustable by setting different external division resistors, while TPS63001 and 002 have fixed output voltage, and FB pin should be connected to VOUT pin for these two chips.
The fixed output voltage of TPS63001 is 3.3V, but for TPS63002 it is 5V, so I'm afraid customer can't use TPS63002 to replace TPS63001.
Best Regard,
Nathan