Hi,
I am trying to troubleshoot my device. The device was initially designed with the gate and source of the DSG and CHG MOSFETs switched around, with wrong footprints also used for zener diodes used for ESD protection on the SMBUS circuit and the PRES (system present) circuit. Upon initial connection with this design, the system worked after removing the SMBUS zener diodes, and I was able to use the BQEASY software to connect successfully to the device.
However, the device failed after some time, possibly due to the incorrect connections for the DSG and CHG MOSFETs (which were found much later). During this time I got a VB_T2H_NACK error. I have since fixed the connections for the DSG and CHG MOSFETs, and the circuitry of the whole device should now match the one presented in its datasheet.
Nevertheless, I receive a VB_T2H_UNKNOWN error. I am not sure what this is supposed to mean, given that I did not send any commands or change the device in any manner during the short time which it was functional. Is it possible that this error refers to the device being in a SEALED state, and if so, is it possible to obtain the UnsealKey or any other relevant codes to reverse this? And in addition, is there a set of instructions of how to do this using the BQEASY software?
Is it also possible that the device is dead? I am not getting any output from the 2.5 V and 3.3 V regulators of the BQ device, so I suppose that is a possibility? Please advise.
Best regards,
Rizqi