Other Parts Discussed in Thread: TPS796
The TPS795 data sheet has the incorrect information posted in the "6.4 Thermal Information" section. The DRB (VSON) is labeled as having 6 pins, and the DCQ (SOT-223) is labeled as the 8 pin option. This is reverse as to what the rest of the data sheet tells us. I was just hoping to get some clarification as to which column pertained to which package/pin option because they are vastly different values.