Hi Team,
We received this inquiry from our customer.
The LDO on this IC (BQ21061) will power the MCU and other peripherals. In order to program the MCU, I will need to supply the circuit/MCU from an external power source and therefore the LDO pin will also see this voltage.
I want to make sure that this external voltage will not damage the IC.
From the datasheet, I can't really tell with certainty that it will not since this voltage is feedback to other parts of the IC.
I need to connect an external voltage (~3V) to the OUTPUT of the LDO(LS/LDO pin) and not the input to program the MCU. The IC charger will not be powered on during this process. I want to know if this will damage or cause any issues because we don’t have access to the Vin pin on the charger IC.
Can you please confirm if this is possible without damaging the BQ21061?
Regards,
Danilo