This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM62440-Q1: Question on Cff

Part Number: LM62440-Q1


Hello,

How should I choose the Cff capacitor value?

I plan on using the adjustable output voltage option in my design (LM62440APPQRJRRQ1). The design will have 12V input and 9V output. Max output current is 2.4A. Since the duty factor is VOUT/VIN, then the duty factor is 75%. As a result, I used equation 9 in the datasheet to calculate the minimum inductance for L1 and chose L1 to be 2.2uH:

I wanted to ask how to determine Cff for best transient performance in the given adjustable voltage setup? For now, I set C293 to be 22pF.

Best,

Justin Phan