Hi
I am testing the BQ25895EVM .
Question
In datasheet, pulse occurs when INT pin is below. However, there is no change when measured by EVM
How is the INT (TP15) of the EVM measured?
-Datasheet(P.25)-
The INT notifies the system on the device operation. The following events will generate 256-µs INT pulse.
• USB/adapter source identified (through PSEL or DPDM detection, with OTG pin)
• Good input source detected – VBUS above battery (not in sleep) – VBUS below VACOV threshold – VBUS above VVBUSMIN (typical 3.8 V) when IBADSRC (typical 30 mA) current is applied (not a poor source)
• Input removed • Charge Complete • Any FAULT event in REG0C
Thanks