This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5118: FB function inquiry.

Part Number: LM5118

Hi

My customer is conducting a test to control the FB pin with an external signal.
The connection was as follows.
DC Supply (#1) : Input 53V
DC Supply(#2) : FB 2V

However, if DC 2V is applied to the FB pin, the LM5118 dies.
Is there a problem with the test method?
The SCH is as follows.

Thanks