TI experts,
1. My MOSFETs are set to series mode.
2. Settings:Protection:Body Diode Threshold Set to 6000mA or 600mA, load 6.5A high current discharge, unable to turn on charging FET (CFET).
3. I would like the CFET to be automatically enabled on discharge at 6.5A, to prevent thermal damage to the CFET's diode. How should I set the parameters?
bq76952-6.5A-Discharge-2022-5-25.xlsx
bq76952-0-36-10bei-0.143mR-R00-2022-5-22(CRC).gg.csv