Other Parts Discussed in Thread: GPCCEDV
Hi Ti
I am using bq34110EVM-796 Evaluation Module connected as below.
Using this for Lead Acid Battery. (12V@ 12AH).
I had configured all the values in data memory of chip, using BQ studio.
After configuring i can get the 'Time to empty' and 'Average time to full' and other parameters.
Now below are my Queries
1) Why do i need the Learning Load?
2) What is the purpose of Learning Load?
3) If I disconnect the battery, when Relative state of charge is 0%, and if i re-connect the same battery its showing full charge as per below image? why it is show full charge and what should i do to get the previous profile.
4) How to choose Learning Load. for this bq34110EVM-796 Evaluation Module? is it ok if i use Fan (5W) as Learning Load?