This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24160: Fault using IN src around 75% charge

Part Number: BQ24160
Other Parts Discussed in Thread: BQ500212A

When using the IN source I see faults at just below 4.1V.  About 75% capacity.  My charge current is 300mA.  It will charge for some number of seconds(3-20) then fault and repeat.  The net effect is a very slow charge.  If I drop the charge current to anything lower the process is similar but the charge/discharge ratio is fairly even and it just hovers at 75% capacity.  When I use the USB source my current is above 500mA and charging appears just fine.

I'm unclear why it faults on the IN source.  When the battery is below the 75% threshold I can drop the current as long as I stay above the 75mA threshold mentioned as the current sink for the IN source.  Charging works normally until I hit just below 4.1V. It seems close to the DPPM threshold of 4.2 so I suspect that is related but I'm not sure.


Even when I have a >300mA IN source why does the current drop so much to cause continuous faults?