Hi,
I have a question concerning the maximum output voltage of LM5156 IC.
On the link below, it says that Vout(max) is equal to 300V. On the other hand, using Webench Desinger maximum output voltage that can be chosen is 500V and for the following parameters design can be normally created:
Vin(min) = 48V, Vin(max) = 52V ; Vout = 410V, Iout = 0.05A.
Here is the link: https://www.ti.com/product/LM5156
So, can I use LM5156 for output voltages exceeding 300V?
Regards,
Mateo