Other Parts Discussed in Thread: LM5121
Hi there,
I have implemented a 55V 5A boost converter design using the LM5121 (stepping up from ~30-42V battery input voltage).
However, the design will not start switching - I only get the input voltage on the output. This indicates the disconnect MOSFET is working correctly, and I can see the gate does indeed have a voltage ~ 10V higher than V in.
Similarly, the bootstrap capacitor on the output has the expected voltage of ~ 10V higher than V in.
When I probe the Soft Start pin, I can see the converter starts to turn on, as the voltage on the capacitor starts ramping up. However, part way through the ramp it resets back to zero volts. As a result, I see a triangle wave on the soft start pin.
I have tried several different soft start capacitor values, and restart capacitor values (including tying reset to ground) but the regulator will not start switching.
Any ideas as to what may be the issue?
Thanks!