This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7H2201-SP: TPS7H2201-SP won't disable output

Part Number: TPS7H2201-SP

Hello,

I am using the TPS7H2201-SP component and I am unable to switch off the load. I have a 5V input, when I turn the enable low my output only reduces to 1.3V

This is my implementation. The enable signal has no noise. I measured some of the other pins when EN = 0V

CS: 0.1V

OVP: 0.49V

RTIMER: 0V

IL: 0.113V

ILTIMER: 0V

SS: 5V

VOUT: 1.3V

The device turns on as expected.