Other Parts Discussed in Thread: CSD17507Q5A, , TPS40304, CSD17501Q5A, CSD17506Q5A
Hi,
We have designed a circuit around the TPS40305DRCR.
Vin = 9V to 16V. Vin is connected to an external battery.
Vout = 5V/8A.
The MOS are CSD17507Q5A.
/resized-image/__size/320x240/__key/communityserver-discussions-components-files/196/P5V.jpg
At power up, there is no high load on the P5V supply (except capacitors).
We have two boards where the low side MOS is broken (short circuit state) just after the power up. No load has been added on the P5V. The current consumption is normally less than 2A.
Could you analyse our schematic to find what is wrong?
The CSD17507Q5A is died in short circuit. Is it due to an over current or an over voltage?
CSD17507Q5A is not a good choice for this application?
BR