Hi Team,
I am using the TPS62745 regulator and have the input ~ 8.7V and output voltage set to 3.3V. The output is regulated at beginning without load, however when the 10mA load is connected out voltage is dropping to 0.V, it seems to fail the regulation with lower load,Can I have some help to understand why this is happening please?