This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27742-G1: BQ27742-G1

Part Number: BQ27742-G1


Hi,

I'm currently working on BQ27742, I achieved shutdown mode using this. I wanted to try Full Sleep mode.  I tried different methods as mentioned in reference manual. But, not successful in achieving current as mentioned in datasheet. The methods which I followed are below,

1. Sleep current=15mA, FS wait=0, entered manually into full sleep by giving FULL_SLEEP command.

2. Sleep current=1mA,FS wait=5, tried to see whether Full sleep is achieved automatically.

Not achieved required current. Sometimes, when I used 1st point I achieved full sleep current, but not always. And the current is varying for every second. Not as mentioned in datasheet for every 20secs. And the range of current is 65uA - 300uA for every 2 secs.

How can I achieve Full sleep?

Thanks in advance,

Kavya.