This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54201: Driving a Peltier Element (TEC) with the TPS5401

Part Number: TPS54201

Hi,

Application Report SLUA979A describes a circuit using the TPS54201 to drive a Peltier Module (TEC) in constant current mode as opposed to PWM mode. However, the circuit using the TPS54201 is unidirectional and can therefore drive the TEC to either heat or cool but not both. Would it be possible to insert an H-Bridge into this circuit as shown in the schematic below to achieve bidirectional control of the TEC for both heating and cooling?

Regards,
James