Hello TI Team,
From the datasheet , i understand that the Fault pin will be internally pulled low with a constant current source in the range 500-1000 uA.
Q1. If it is a constant current source, then why we have a range of values?
Q2. Consider Fault pins of two TPS92611-Q1 are connected together and is connected to Microcontroller for external control. I need to pull up the fault pin instead of floating. How i can regulate the pullup current < 500uA (minimum of pull down current source)
Thanks in advance