Other Parts Discussed in Thread: TPS63901, TPS63810
Hi Team,
I am looking for a lower current alternative to TPS63811.
max current needed is 20mA, a fine regulation within the requested range is a must have.
Input voltage: from 2.4V to 4.2V
Output Voltage: from 2,7V to 3,2V
Output current range : from 0 to 50mA
What would you recommend here?
BR,
Stefan