Hi all,
I have two more questions on the TPS65023 I2C.
1. I would like to use i2c to control the output voltage of DCDC1. Beside setting Core adj allowed bit in CON_CTRL to 0 and setting COREx in DEFCORE to [0, 0x1F], is there something else that I need to config?
I am able to control the output voltage of LDOs by setting LDO_CTRL register, but fail to do so with DCDC1.
2. Although the datasheet suggests to pull up the I2C bus to VRTC(3V), what happens if I pull up the I2C bus to other voltage like 3.3V? What will tps65023 i2c response to that 3.3V?
Is it necessary to add a voltage shifter there in this case?
Regards,
Leung