Part Number: TPS62060
Hi team,
Customer wants to comfirm the state of output impedance when the input voltage is zero. Is it Hi-Z?
They use this deivce at 5Vin, 3.3Vout. Then, they want to make the vout keep 3.3V at certain time after the input voltage is lost due to some reason. So they consider to add a cap on input line or output line. They aslo take care about the reverse current. Therefore, if the output impedance will become Hi-Z, they cosider to add the cap on the output. If the output is not Hi-Z, they consider to add the cap on the input.
Could you give any advice on this?
Regards,
Noriyuki Takahashi