Other Parts Discussed in Thread: TPS65023
Hello,
We are planning to use TPS65023QRHARQ1 PMIC to power-up the system with nxp's IMX6ULL processor and our system.
Input supply VIN = 5V.
Schematic diagram is attached below.

Query 1: Can we connect the PMIC pin#27 RESPWRON to the processor POR pin for proper operation of the system?
Query 2: PMIC pin#14(VSYSIN) and 15(VBACKUP) are shorted to ground in our schematic. Will it provide 30mA output on VRTC output with this configuration or any other configuration is required?
Query 3: What would be the initial output voltages on each buck regulator output at time of power-up?
Query 4: For POR functionality, any other pins from PMIC can be used?
Query 5: Is PWRFAIL output is similar to PGOOD output?
Thank in advance!