This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR33640: wave soldering

Part Number: LMR33640
Other Parts Discussed in Thread: TPS5420, TPS54331

Hello,

Our customer is looking for a DCDC converter to meet following spec, and found out LMR33640 is the best. However I do not know LMR33640 can support wave soldering. Could you let me know if LMR33640 can support wave soldering.

- DCDC1

Vin=15V to 20V,

Vout=10V to 13V, Iout=3.5Amax, Efficiency should be higher than 95% at 5W (0.38A to 0.5A)

wave soldering capability is necessary.

- DCDC2

Vin=15V to 20V

Vout=3.45V, Iout=1A

wave soldering capability is necessary.

Best regards,