This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP5030: The RED LED will keep on...

Part Number: LP5030

Dear Sirs,

My customer feedback the LP5030 cannot turn off the red LED.

1. After customer function testing ok, the products were stored in stock. However, after some period and customer test again and found the red LED can't turn off.

The Vled is 5V and for the NG port, the OUT pin will be 3.1V and the red LED turned on. (the good port is 3.9V.)

2. change another LP5030 and the issue is fixed.

3. customer tries to set the Vled to 4.5V, but the red LED still keeps on. (the OUT voltage will decrease, too)

4. there are 2pcs LP5030 per board, and only 1 pcs will fail at the same time and will not change.(NG will not recover)

5. while the issue occurs, customer still can control LP5030, but can't display the correct color. 

 G  B  W

6. the registers setting, schematics, layout as below.

0x40, 0x3C, 0x00, 0x00, 0xFF, 0x00, 0x00, 0x00, 0xFF, 0xFF,

0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF,

0x16, 0x16, 0x16, 0x16, 0x16, 0x16, 0x16, 0x16, 0x16, 0x16,

0x16, 0x16, 0x16, 0x16, 0x16, 0x16, 0x16, 0x16, 0x16, 0x16,

0x16, 0x16, 0x16, 0x16, 0x16, 0x16, 0x16, 0x16, 0x00, 0x00,

0x00, 0x00, 0x00, 0x00, 0x00

LP5030RJVR LED Driver.pdf

Left: 

Right:

Please help to input your comments or the IC is damaged.

Thanks.